Other Parts Discussed in Thread: IWR1642
Hello,
at the PPL Counting lab there are two different cfg files with the following parameters:
Maximum range: 6.3 meters / 14 meters
Range resolution 5.5 cm / 12 cm
Maximum velocity 23.6 Km/h / 23.6 Km/h
I would say the maximum velocity values should be m/s and not km/h.
Could you please check that for me again? And if my calculations are wrong, could you show me how to do the math correctly.
Thanks in advance!
Nicolas