This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: LVDS interface tolerances

Part Number: AWR1243


According to the AWR1243 datasheet at "5.9.5 LVDS Interface Configuration", (and the AWR1xx_Radar_Interface_Control-doc at "5.16.5 Sub block 0x4044 – AWR_DEV_RX_DATA_PATH_CLK_SET_SB"), the LVDS interface supports only fixed data rate.

Are there any numbers that TI can present on who much we can expect these data-and-clk rate, on the LVDS-interface, to wary within?

E.g.:  LVDS_CLK = 300 ± ? MHz => which gives us an expected datarate LVDS_TXP/M = 600 ± ? Mbps

B.R.
/Henric