Hi TI Team,
I want to ask a question about the value of resistor R85 and R92 in IWR6843ISK schematic.
R85=12.1k
R92=48.7k
Could I change other resistors to replace these two resistors because these value of resistor are hard to find?
I guess the resistors are for dividing voltage. I think I need to meet the rule of R85/R92=12.1/48.7=0.248. So if I choose the R85 equal to 1k ohm. 4k ohm can be chosen on R92.
Is it right?
Look forward to your response,
Lukas