This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: SPI interfaces to FPGA

Part Number: AWR1243

Hi

According to AWR1243 device sheet ,SPI and other control interfaces are serially connected to resistance .Is it possible to connect directly to the I/O port of FPGA without a resistance?(both AWR1243 and FPGA interface power supply is 3.3V)