This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: Can mmwave studio config complex 1x and 2x at the same time?

Part Number: AWR1243

ADC has 3 formats:real ,complex 1x , complex 2x.

Can i config a frame with those 3 formats?

For example:

a frame with 3 chirp  has 64 num loops, that is chirp0_chirp1_chirp2__chirp0_chirp1_chirp2__chirp0_chirp1_chirp2....

chirp0 is real adc format

chirp1 is complex 1x adc format

chirp2 iscomplex 2x adc format