LDC1314 is used at out mass production as below link, in order to sense copper ball approaching.
https://dendama.co.jp/gummy.html
Under the sun, the output of LDC 1314 is stopped. Are there any issue, when the sun lights LDC1314 IC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LDC1314 is used at out mass production as below link, in order to sense copper ball approaching.
https://dendama.co.jp/gummy.html
Under the sun, the output of LDC 1314 is stopped. Are there any issue, when the sun lights LDC1314 IC?
Hello Dendama-san,
The LDC1314 could be overheating if it is operating at temperatures greater than 125 degrees Celsius (the maximum operating temperature listed in the datasheet). Are you able to measure the temperature when the output stops?
Best Regards,
Hello Dendama-san,
A useful LDC debugging technique is to get an oscilloscope and look at the sensor signals and check the frequency and voltage. Perhaps the sensor was not configured properly for the range of Rp.
Regards,
ChrisO
Under the sun, the device is not responding at all for a few seconds. Once the device goes back to the place where is non sun light, the device is responding again. But, in this case, the output value is something wrong.
Look at either the INAx or INBx (where x is the channel number the sensor is attached to). You can either look at INAx to ground or INBx to ground; or if you have a differential probe, you can look INAx - INBx.