Other Parts Discussed in Thread: LM96163
Hi there
I have spent way to many hours by now to get this EVM to work. I had the drivers installed as described in the User's Guid (Chapter 3).
It still doesn't show up in the device-manager as described in Figure 26. It appears as a generic device.
So, I don't even know if my computer can properly establish communication with the EVM.
Regardless, I was trying to set the registers of LM96163 through the GUI and read them back. But everytime they jump back to "0".
Also, I assume if there was a connection to the LM96163 I should be able to plot at least the temperature-curve. But nothing happens there either.
What else can I do to get this thing working?
Thanks in advance