This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Missing Characters from mmWave_Demo_Visualizer

Part Number: AWR1642

Dear Officer,

We are using SDK2.1 running on AWR1642, and using mmWave_Demo_Visualizer  for our testing. When we try to use " LOAD CONFIG FROM PC AND SEND" option under plot, ver often we got missing chraters in the control port hence the device can not be start correctly. e.g.in the configuration file:

"lowPower 0 1"

But our device only got "Power 0 1" hence it will be treated as wrong command.

We did modify some algorithm but we don't touch on the cli.c tasks poart. Any suggestions why we can't get miss characters when receiving from control port from  mmWave_Demo_Visualizer? It is the loading too fast from mmWave_Demo_Visualizer? 

Tks and best regards

He Wei