This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91051: LMP91051 issue need help

Part Number: LMP91051

Hi Sir

We are now preparing to develop a dual-channel carbon dioxide sensor based on LMP91051. Please ask a few questions:

1. What are the parameters of address 0x0 and 0x1 set according to?
2. Is there any actual effect of the external bandpass filter on the A0 and A1 pins? What is the external filter based on?
3. Do you have to add an op amp to the temperature measurement circuit?
4. What is the purpose of measuring the voltage of the CMOUT pin?
5. How is the carbon dioxide concentration obtained?
6. What is the best time to sample AD after switching channels?