This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: What would be main difference between awr1843 and iwr6843?

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843, AWR1843

What would be main difference between awr1843 and iwr6843?

We would like to use awr1843 power rail(schematic) for iwr6843 to support 5V DC jack. Would it be good idea? 

Thanks for your answer in advance,

  • Hello,

    You could re-use the AWR1843 power rails to IWR6843 to support 5V DC jack.
    However other areas such as RF traces and Antennas are designed for 60GHz for IWR6843 and AWR1843 devices it's designed for 77GHz frequencies.
    Supported flashes are different between IWR6843 and AWR1843.
    If you are developing custom board then recommendation to use same flash family that is present in respective EVMs.

    Thanks and regards,
    CHETHAN KUMAR Y.B.