Other Parts Discussed in Thread: FDC1004
Hi,
I am using an FDC1004evm device for object detection. one of my measurement i took almost 9000 samples and contains high noise from my sensing environment.
When I try to plot these samples in Matlab and try to make the frequency spectrum its shows the peaks only near 0 to 5Hz. (Sampling frequency was 95 Hz).
Actually, my question is is there any reference signal I can compare with? ls, there any frequency spectrum with the target?
Thanks in advance.