Other Parts Discussed in Thread: TIDEP-0091
IWR1443 experts,
Could you please help with some specific details on power consumption with the IWR1443? A customer wants to detect the presence of an object 1 m away. The object is very large and made of steel. The application can be based on the TIDEP-0091.
http://www.ti.com/tool/TIDEP-0091
Low power is critical in this application so the MCU + IWR1443 will stay in a low power mode most of the time, then wake and take a measurement.
I looked at the Power calculator, but I don't have the numbers needed to enter there. So, ...
How much power does the IWR1443 consume in low power mode? (I didn't see this in the datasheet).
How long does it take to wake from low-power mode up until taking a measurement?
How long would a single distance measurement take, as I've described above?
Thanks,
Darren