This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: IWR6843 peoplecounting configuration file

Part Number: IWR6843

Hi Team,

Customer wants to know what is the meaning of this configuration file?

*************************************************************************************

flushCfg
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg 0 1 1 1
profileCfg 0 60.6 30 10 62 0 0 53 1 128 2500 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
frameCfg 0 1 128 0 50 1 0
lowPower 0 1
guiMonitor 1 1 0 0
cfarCfg 6 4 4 4 4 16 16 4 4 55 67 0
doaCfg 600 1875 30 1 1 0
SceneryParam -6 6 0.5 6
GatingParam 3 2 2 0
StateParam 10 5 100 100 5
AllocationParam 250 250 0.25 30 1 2
AccelerationParam 1 1 1
trackingCfg 1 2 250 20 52 82 50 135
sensorStart

  • Hi Annie,

    "flushCfg
    dfeDataOutputMode 1
    channelCfg 15 5 0
    adcCfg 2 1
    adcbufCfg 0 1 1 1 
    profileCfg 0 60.6 30 10 62 0 0 53 1 128 2500 0 0 30
    chirpCfg 0 0 0 0 0 0 0 1
    chirpCfg 1 1 0 0 0 0 0 4
    frameCfg 0 1 128 0 50 1 0
    lowPower 0 1
    guiMonitor 1 1 0 0" -> see SDK user's guide

    "SceneryParam -6 6 0.5 6
    GatingParam 3 2 2 0
    StateParam 10 5 100 100 5
    AllocationParam 250 250 0.25 30 1 2
    AccelerationParam 1 1 1
    trackingCfg 1 2 250 20 52 82 50 135" -> see People Counting Customization guide

    "cfarCfg 6 4 4 4 4 16 16 4 4 55 67 0
    doaCfg 600 1875 30 1 1 0" -> this E2E post

    Regards,

    Justin