This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST : awr1642 Interference between two instruments

Part Number: AWR1642BOOST

Hello.

I'm using two awr1642s to combine radar images to increase resolution.

Before we went into the work, we found out that there were interference effects on many machines.

And also, we've seen a number of ways to get rid of interference through mmwave studio.

However, when I ran two devices and I saw the x-y scatter plot achieved using the visualizer, we thought there was no interference between the two machines.

The reason why we thought there was no interference here was because we could see that the dots on the scatter plot were almost identical to the number and location of objects.

1. Why can't we see any interference between the two machines?

2. Is it because one of the reasons for question 1 was not to run through the studio but simply to obtain the radar image through visualizer?

Thanks, in advanced,

Regards,