Other Parts Discussed in Thread: UNIFLASH, , MMWAVEICBOOST
Hi,
I tried on IWR6843ISK+MMWAVEICBOOST board, the binary can be download through xds110 user port with S1 in default mode, I noticed the RS232_TX/RX are also connected to FTDI chip, I changed the S1.5 to OFF, S1.7 to ON, connected the FTDI_USB with micro usb port, 4 USB port can be emulated on PC, choose the 3rd port for flash burn in uniflash tool, but failed.
Switch to use radar studio then RS232 can be connected through FTDI 3rd port, and the BSS/MSS binary can also be downloaded well in radar studio.
So my question is how to download image in uniflash through the FTDI RS232 port?
Andy