Part Number: TDC1000-TDC7200EVM
I want to make a flow measurement placing the sensors like the Z-mount shown in the picture but as far as now I did not have success. With that I'm wondering if there is any limitation to do that with the TDC100-TDC7200EVM board, or maybe have problems with my experimental setup, where I just glued the sensor in a 45° angle direct on the pipe.