This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA305: Calibrating PGA305 with USB2any

Part Number: PGA305
Other Parts Discussed in Thread: USB2ANY

Hello

We have the PGA 300EVM and PGA305EVM and developed a little PCB with the PGA305. Now I have problems to calibrate the PGA305. I connected our PCB with the USB2any via i2C, without using the EVM. Is this possible? I can read the parameters of the PGA but not write and calibrate the PGA. When I want to use the guided calibration it says that I2C is not active, even when it was active before and I could read the EEPROM.

What is wrong?

Can somebody help with the calibration of a load cell setting Zero and gain?

Thank you very much.