This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/PGA900: How to run a program in PG900EVM without debugging

Part Number: PGA900
Other Parts Discussed in Thread: UNIFLASH,

Tool/software: Code Composer Studio

Hi all.

I'm reading a lot of posts about this topic but I can't achieve that my program run after power on reset corectly.
I can compile with TI v18.1.5.LTS and run my code with CCS  8.3.1.00004 without any problem but if I want to put this code in DEV RAM zone, after a power reset the program doesn't run.
This is my normal procedure:

  • Jumper 15 connected. 7,5VDC arrives correctly to VP OTP Pin.
  • With PGA 900 utility:
    • Send 3 to MICRO_INTERFACE_CONTROL
    • Send 0 to REMAP
    • LOAD .hex to OTP Memory
    • LOAD the same .hex file to Dev RAM
    • Click to REMAP Enabled (or send 1 from low level configuration menu)
    • Send 0 to MICRO_INTERFACE_CONTROL (or change to microcontroller interface.)

After this actions, the program runs but after remove my external VCC (24VDC) the program not run.
Anybody knows what can I do to run my code correctly?
I've tried with UniFlash 5.0.0 but the problem is the same. I can program mi device but at the end it doesn't run.

Thanks in advance team.

Regards

  • Hello,

    There is no need to program the DEVRAM and change the REMAP if your goal is to program the OTP. When you program the OTP using the PGA900EVM GUI do you also verify the OTP afterword to make sure that it was programmed properly?

    Do you remove the 7.5V to the VP_OTP pin after programming and before resetting the device?

    Regards,
  • Hi Scott.

    Thanks for your reply.

    According to the first question: With PGA utility, after programming my OTP Memory I'm going to verify this memory. The result of this verification goes into a PGA900_Verification_Log.txt. I've attached this file. I think that It's ok but I don't know if it's true or not.

    On the oher hand, I tried all the posibilities with this Jumper :) 

    I think that the procedure that you refer is:

    • Close jumper 15.
    • Turn on external VCC. I have 24VDC
    • Open PGA900 utility.
    • Move to a Digital interface: This accion, put the microcontroler on Reset State.
    • Send 0 to REMAP register
    • Load .hex to OTP memory
    • Load .hex to Dev RAM
    • Send 1 to REMAP register
    • Remove jumper 15
    • Move to a Microcontroller interface (the program runs).
    • Turn off external VCC
    • Turn on externall VCC (the program doesn't run).

    Do you have more ideas?  I've verified that SECLOCK were in 0 and DEBUG_LOCK in micro interface control register were in 0.

    I think that it's a normal procedure to program the microcontroller, isn't it?

    Thanks again.

    Regards

    Reg Address	Hex File Data	Device Data
    4	163	175
    8	169	189
    12	173	189
    16	171	191
    20	171	191
    24	171	191
    44	171	191
    48	171	191
    56	171	191
    60	171	191
    64	17	29
    68	1	13
    72	171	191
    76	65	77
    80	171	191
    84	171	191
    88	171	191
    92	171	191
    96	171	191
    100	171	191
    104	171	191
    108	171	191
    112	171	191
    116	171	191
    120	171	191
    124	171	191
    128	171	191
    132	171	191
    136	171	191
    140	171	191
    144	171	191
    148	171	191
    152	171	191
    156	171	191
    160	171	191
    164	171	191
    168	171	191
    172	171	191
    176	171	191
    180	171	191
    184	171	191
    188	171	191
    197	38	39
    200	96	99
    202	97	101
    204	6	7
    222	93	125
    224	120	122
    225	79	95
    226	10	11
    227	26	58
    228	1	65
    229	32	98
    230	64	80
    231	66	98
    232	16	94
    233	96	104
    234	91	95
    235	72	74
    237	74	90
    238	8	10
    239	26	122
    240	2	94
    241	96	106
    243	74	106
    244	62	126
    245	128	200
    246	66	74
    247	96	122
    249	72	104
    250	113	241
    251	77	79
    252	10	26
    253	26	122
    254	2	95
    255	32	104
    256	192	207
    257	67	99
    258	16	18
    259	96	224
    260	88	92
    261	72	74
    262	79	95
    263	34	106
    264	2	18
    266	88	124
    267	74	106
    268	88	92
    269	72	74
    270	1	193
    271	35	99
    274	52	124
    275	32	104
    277	74	106
    278	192	194
    279	67	195
    280	16	91
    281	128	202
    282	87	95
    284	7	23
    285	34	162
    286	2	94
    287	128	200
    288	86	247
    289	74	106
    291	72	200
    292	97	123
    293	76	78
    294	16	21
    295	128	160
    296	86	214
    297	72	75
    298	161	177
    299	34	162
    300	2	91
    301	128	200
    302	86	94
    304	5	21
    305	32	160
    306	192	198
    307	67	99
    308	16	90
    309	128	202
    310	86	214
    311	72	75
    313	74	202
    314	99	123
    316	16	23
    318	134	222
    319	32	104
    320	84	85
    321	74	110
    322	192	199
    323	67	195
    324	16	89
    325	128	200
    327	72	106
    328	16	20
    329	34	114
    330	6	95
    331	128	200
    332	83	91
    333	72	75
    335	97	113
    336	6	94
    337	128	202
    338	83	91
    340	174	191
    341	97	225
    342	3	31
    343	112	240
    344	82	87
    345	72	104
    346	238	239
    348	2	90
    349	112	120
    350	82	94
    351	74	79
    352	83	87
    353	72	200
    354	22	94
    355	128	200
    356	38	47
    358	6	7
    359	96	112
    360	70	87
    361	96	104
    362	82	90
    363	72	77
    364	46	47
    365	98	226
    366	6	87
    367	128	200
    368	81	127
    369	72	120
    370	174	255
    371	96	109
    372	6	199
    374	81	87
    375	72	105
    376	46	111
    377	112	113
    378	6	135
    379	128	225
    380	62	255
    381	112	113
    382	83	87
    383	79	111
    384	46	175
    386	59	63
    388	1	45
    389	39	119
    391	2	39
    392	23	127
    393	128	130
    394	1	21
    395	34	162
    396	146	147
    397	2	34
    398	2	83
    399	39	111
    400	34	178
    401	128	130
    402	36	62
    403	34	162
    404	78	110
    405	76	110
    406	82	83
    408	144	152
    410	20	29
    412	77	93
    413	76	77
    414	79	95
    415	74	75
    416	172	173
    418	42	43
    420	76	79
    421	76	77
    422	78	95
    423	74	75
    424	236	237
    426	78	95
    427	76	77
    428	19	31
    430	34	43
    433	96	102
    434	58	59
    438	34	43
    440	75	79
    441	74	75
    442	76	79
    443	76	77
    444	19	31
    447	34	35
    448	226	235
    450	102	111
    452	35	47
    454	74	79
    455	76	77
    457	35	39
    458	27	127
    460	31	63
    464	223	255
    467	35	39
    468	73	77
    470	35	47
    472	36	37
    473	35	39
    474	33	59
    475	36	109
    476	94	95
    480	10	11
    482	68	71
    484	174	175
    488	46	62
    489	76	110
    490	10	11
    492	66	71
    494	16	48
    495	34	110
    508	16	18
    510	248	250
    514	253	255
    515	32	99
    516	16	242
    517	64	122
    518	248	250
    520	32	242
    521	120	122
    522	0	242
    523	7	127
    524	16	18
    525	209	211
    526	72	250
    527	28	126
    528	192	240
    529	178	250
    530	4	28
    531	40	104
    532	0	240
    533	219	251
    535	70	126
    537	112	119
    538	129	147
    539	0	209
    540	64	72
    541	70	94
    542	64	192
    543	88	250
    544	128	132
    545	71	111
    547	120	251
    548	0	56
    549	7	71
    550	2	43
    551	209	217
    552	32	104
    554	0	129
    557	208	214
    560	33	161
    561	72	79
    562	0	32
    565	40	47
    567	208	209
    568	31	63
    569	72	120
    571	112	119
    572	31	255
    573	72	216
    574	2	35
    575	136	200
    576	48	113
    577	72	120
    578	80	120
    579	64	120
    581	74	106
    582	16	215
    583	128	208
    584	214	223
    585	231	239
    586	192	239
    587	70	118
    588	4	6
    589	5	141
    590	0	48
    591	64	72
    592	35	115
    593	5	69
    594	0	46
    595	64	74
    596	163	179
    597	34	162
    599	95	255
    600	35	39
    601	33	37
    604	0	35
    605	0	5
    607	128	192
    608	192	227
    609	192	226
    610	192	255
    611	192	223
    613	36	37
    618	0	64
    619	32	160
    620	74	202
    621	1	193
    622	0	192
    623	32	224
    624	72	107
    626	0	255
    627	0	95
    632	82	90
    637	1	45
    640	208	214
    641	166	167
    644	88	90
    648	84	92
    652	78	222
    653	1	167
    654	0	255
    655	32	255
    656	173	253
    659	0	32
    660	90	94
    664	68	78
    668	70	239
    669	1	71
    672	93	95
    680	64	70
    684	66	95
    688	52	124
    704	0	72
    708	6	94
    712	95	127
    720	61	63
    721	4	5
    723	0	32
    724	191	255
    727	0	32
    728	65	97
    731	0	32
    732	9	73
    733	3	7
    736	26	219
    737	2	3
    740	25	93
    741	2	3
    744	11	31
    745	4	7
    748	56	58
    749	5	7
    752	244	253
    753	4	6
    756	39	47
    760	41	57
    764	14	254
    765	2	6
    768	4	39
    769	4	5
    775	0	64
    777	72	74
    780	2	6
    781	120	124
    784	17	255
    785	67	255
    789	33	105
    791	112	120
    793	33	121
    795	112	120
    796	129	145
    797	120	123
    798	106	107
    799	74	218
    800	17	255
    801	112	113
    804	0	3
    806	1	65
    807	208	240
    809	33	121
    810	129	235
    811	112	122
    812	103	119
    813	73	121
    814	8	137
    817	34	43
    818	80	81
    819	64	208
    820	8	255
    821	112	113
    822	102	231
    823	73	121
    824	8	111
    825	120	121
    826	80	88
    827	64	120
    828	8	9
    829	112	114
    833	181	245
    834	100	102
    836	6	14
    837	32	120
    838	100	116
    840	67	75
    841	94	126
    842	0	112
    843	32	103
    844	20	60
    845	94	255
    846	96	100
    847	74	75
    848	21	23
    850	92	124
    851	67	75
    852	173	239
    853	0	94
    855	25	57
    856	236	252
    857	97	127
    858	20	116
    859	120	122
    860	164	181
    861	0	120
    862	12	92
    863	25	91
    864	21	189
    866	228	237
    867	105	121
    868	173	237
    869	0	97
    870	164	180
    871	19	123
    872	77	237
    875	97	121
    876	20	21
    878	91	255
    879	77	109
    880	164	173
    882	12	172
    883	25	27
    884	45	109
    885	94	95
    886	228	236
    888	44	60
    889	25	121
    890	21	95
    891	120	125
    896	236	237
    897	97	127
    898	20	244
    899	120	121
    900	164	172
    901	0	25
    902	12	29
    903	25	121
    904	228	237
    906	92	93
    907	67	91
    908	19	255
    909	120	121
    910	155	159
    911	0	120
    912	203	239
    915	97	121
    916	19	247
    917	120	121
    918	155	223
    919	0	67
    920	203	219
    921	24	120
    924	20	223
    926	155	223
    927	19	115
    928	164	183
    929	0	120
    930	12	159
    932	227	235
    933	97	121
    934	19	219
    935	120	121
    936	77	93
    937	76	124
    939	0	19
    940	203	239
    942	219	223
    943	105	121
    944	32	227
    945	94	127
    946	18	19
    948	192	205
    949	24	92
    950	146	155
    952	137	203
    954	200	219
    955	97	105
    957	189	255
    958	56	58
    959	181	253
    960	68	196
    961	73	89
    962	6	150
    964	71	207
    965	74	90
    966	67	203
    967	94	127
    968	0	56
    969	32	189
    970	20	60
    971	94	255
    972	64	68
    973	74	75
    974	21	23
    976	92	95
    977	67	75
    978	173	239
    979	0	94
    981	25	57
    982	108	124
    983	97	127
    984	20	84
    985	120	122
    986	164	181
    987	0	120
    988	12	92
    989	25	91
    990	21	189
    992	100	109
    993	105	121
    994	173	237
    995	0	97
    996	164	180
    997	19	123
    998	77	237
    1001	97	121
    1002	20	21
    1004	62	126
    1005	77	109
    1006	164	173
    1008	12	172
    1009	25	27
    1010	45	109
    1011	94	95
    1012	100	108
    1014	44	60
    1015	25	121
    1016	21	63
    1017	120	125
    1022	108	109
    1023	97	127
    1024	20	116
    1025	120	121
    1026	164	172
    1027	0	25
    1028	12	29
    1029	25	121
    1030	100	237
    1032	92	93
    1033	67	91
    1034	19	127
    1035	120	121
    1036	155	159
    1037	0	120
    1038	203	239
    1041	97	121
    1042	19	119
    1043	120	121
    1044	155	223
    1045	0	67
    1046	203	219
    1047	24	120
    1048	91	219
    1050	20	223
    1052	155	223
    1053	19	115
    1054	164	183
    1055	0	120
    1056	12	159
    1058	99	235
    1059	97	121
    1060	19	91
    1061	120	121
    1062	49	53
    1063	76	124
    1065	0	19
    1066	203	239
    1068	91	95
    1069	105	121
    1070	32	99
    1071	94	127
    1072	18	19
    1074	192	241
    1075	24	92
    1076	146	155
    1078	137	203
    1080	72	91
    1081	97	105
    1083	189	255
    1084	44	62
    1085	74	122
    1086	56	248
    1087	181	189
    1088	80	210
    1090	128	137
    1091	17	25
    1092	3	75
    1093	178	243
    1094	0	56
    1095	32	189
    1096	80	124
    1097	96	106
    1098	42	58
    1099	74	255
    1100	20	84
    1101	94	126
    1102	32	160
    1103	74	91
    1104	32	35
    1105	73	251
    1109	67	99
    1110	173	175
    1111	0	74
    1112	77	93
    1113	25	95
    1115	96	106
    1116	20	52
    1117	120	121
    1118	164	181
    1119	0	120
    1120	12	92
    1121	25	91
    1122	21	189
    1124	228	237
    1125	104	121
    1126	173	237
    1127	0	96
    1128	164	180
    1129	19	123
    1130	77	237
    1133	96	121
    1134	20	21
    1136	33	229
    1137	77	109
    1138	164	173
    1140	12	172
    1141	25	27
    1142	228	237
    1143	104	121
    1144	45	237
    1145	94	126
    1146	44	60
    1147	25	121
    1148	21	53
    1149	120	125
    1155	96	104
    1156	20	61
    1157	120	126
    1158	164	172
    1159	0	25
    1160	12	29
    1161	25	121
    1162	228	237
    1164	203	207
    1165	128	153
    1166	92	252
    1167	67	99
    1168	19	23
    1170	155	191
    1172	203	207
    1173	24	25
    1174	220	252
    1175	96	104
    1176	19	219
    1177	120	248
    1178	155	223
    1179	0	67
    1180	203	219
    1181	24	120
    1184	20	223
    1186	155	223
    1187	19	115
    1188	164	183
    1189	0	120
    1190	12	159
    1192	227	235
    1193	96	120
    1194	19	219
    1196	19	23
    1197	76	124
    1199	0	19
    1200	203	239
    1202	219	223
    1203	104	121
    1204	32	227
    1205	94	126
    1206	18	19
    1208	192	211
    1209	24	92
    1210	146	155
    1212	137	203
    1214	200	219
    1215	96	104
    1217	189	255
    1218	192	210
    1219	70	126
    1220	88	216
    1221	5	29
    1222	0	146
    1224	2	139
    1225	1	25
    1226	0	200
    1227	32	96
    1228	95	127
    1229	1	189
    1230	0	192
    1231	32	102
    1232	96	120
    1233	1	5
    1235	32	96
    1236	0	2
    1240	90	95
    1244	88	120
    1252	78	94
    1256	76	92
    1260	74	94
    1264	52	126
    1268	84	92
    1272	82	90
    1276	80	116
    1280	31	95
    1281	72	73
    1283	73	105
    1284	0	82
    1285	136	137
    1287	128	160
    1288	30	94
    1289	72	73
    1292	1	31
    1293	112	120
    1294	112	126
    1295	71	79
    1297	73	201
    1298	112	120
    1300	8	30
    1303	74	107
    1305	48	112
    1306	8	120
    1307	112	119
    1308	28	29
    1310	0	112
    1311	32	181
    1313	94	126
    1314	19	31
    1315	96	106
    1316	4	5
    1317	35	51
    1319	94	126
    1320	83	95
    1321	104	105
    1323	24	56
    1324	26	27
    1325	76	94
    1326	38	55
    1328	83	87
    1329	96	99
    1330	24	220
    1331	75	95
    1332	0	83
    1333	46	110
    1334	29	255
    1335	136	152
    1336	8	26
    1337	208	220
    1338	1	39
    1339	46	126
    1340	4	87
    1341	208	240
    1342	2	26
    1343	46	111
    1345	209	255
    1346	22	31
    1347	72	200
    1349	130	210
    1350	2	3
    1351	224	238
    1352	8	12
    1353	130	210
    1354	0	2
    1355	224	238
    1357	130	211
    1358	20	22
    1361	120	250
    1362	17	19
    1363	104	232
    1364	128	136
    1365	0	130
    1367	24	248
    1368	192	205
    1369	105	235
    1370	65	85
    1371	67	79
    1374	128	145
    1375	0	104
    1376	32	160
    1378	64	96
    1379	105	121
    1380	137	201
    1381	19	123
    1382	64	65
    1383	24	91
    1384	17	57
    1385	104	120
    1386	72	200
    1390	137	201
    1391	0	105
    1392	97	233
    1393	24	27
    1395	104	120
    1396	128	145
    1397	19	123
    1398	8	72
    1399	24	91
    1400	24	57
    1401	128	248
    1402	112	249
    1404	70	103
    1405	1	25
    1406	0	201
    1407	32	104
    1408	36	164
    1409	5	23
    1410	0	8
    1411	64	88
    1413	1	129
    1414	0	112
    1415	32	189
    1416	92	94
    1421	1	5
    1423	32	96
    1424	32	125
    1427	64	96
    1428	72	92
    1432	0	52
    1439	0	64
    1445	42	43
    1447	208	240
    1448	132	255
    1449	70	79
    1452	28	95
    1455	7	39
    1457	209	251
    1458	16	89
    1459	42	250
    1460	8	140
    1461	211	215
    1462	112	251
    1463	180	183
    1464	16	28
    1465	58	251
    1466	120	251
    1467	201	207
    1468	120	122
    1469	192	209
    1473	210	211
    1477	50	58
    1478	56	120
    1479	208	217
    1480	4	124
    1481	42	234
    1482	44	60
    1483	211	251
    1484	8	251
    1485	42	250
    1486	5	117
    1487	211	255
    1488	12	28
    1489	42	58
    1490	1	57
    1492	8	12
    1493	201	235
    1494	8	44
    1495	192	211
    1497	201	235
    1498	8	13
    1499	192	211
    1500	8	12
    1501	201	235
    1502	8	9
    1503	192	211
    1504	146	154
    1505	7	207
    1508	146	154
    1509	15	207
    1510	34	42
    1513	120	249
    1514	3	11
    1515	112	240
    1516	1	147
    1517	49	55
    1518	1	43
    1519	48	240
    1520	1	147
    1521	58	63
    1523	208	240
    1525	7	127
    1527	209	241
    1529	7	55
    1530	20	21
    1531	209	241
    1533	7	63
    1534	216	250
    1536	4	143
    1537	58	63
    1538	18	247
    1540	8	203
    1541	201	207
    1542	3	23
    1543	128	209
    1544	27	155
    1545	12	15
    1546	67	219
    1547	128	208
    1549	48	58
    1550	4	22
    1551	58	251
    1553	210	219
    1554	10	11
    1556	8	27
    1557	201	205
    1558	3	67
    1559	112	240
    1560	27	31
    1561	10	58
    1562	67	71
    1563	112	122
    1564	27	251
    1565	10	218
    1566	131	139
    1567	112	240
    1569	10	203
    1572	4	31
    1573	48	58
    1574	4	71
    1575	58	122
    1576	244	255
    1577	210	218
    1578	4	135
    1579	50	114
    1580	5	31
    1581	208	218
    1582	11	203
    1584	3	7
    1586	1	5
    1587	49	59
    1588	1	245
    1589	48	242
    1590	1	5
    1592	249	253
    1594	96	107
    1595	70	126
    1596	112	115
    1597	71	119
    1598	0	1
    1599	0	49
    1600	248	249
    1602	6	7
    1603	120	122
    1604	0	249
    1605	37	245
    1606	1	97
    1607	48	118
    1608	16	112
    1609	224	231
    1612	1	249
    1613	58	191
    1614	20	22
    1617	50	55
    1618	12	13
    1620	1	17
    1621	49	241
    1622	1	11
    1625	209	251
    1626	3	23
    1627	224	248
    1628	2	3
    1629	120	122
    1630	1	13
    1631	48	112
    1632	10	11
    1633	112	113
    1635	49	59
    1636	118	255
    1637	8	217
    1638	1	3
    1639	53	245
    1640	8	10
    1641	45	125
    1642	234	235
    1643	218	250
    1644	114	122
    1645	8	120
    1647	210	243
    1648	66	118
    1651	120	125
    1653	35	47
    1654	20	254
    1655	9	219
    1656	2	114
    1657	48	56
    1658	63	255
    1659	1	211
    1660	28	94
    1661	64	120
    1662	60	63
    1663	67	123
    1664	19	31
    1665	64	99
    1666	3	23
    1667	51	59
    1669	43	59
    1670	10	63
    1672	2	30
    1674	1	61
    1675	48	115
    1677	10	74
    1678	5	7
    1679	211	243
    1680	7	23
    1681	120	123
    1682	82	90
    1683	6	215
    1684	1	3
    1685	48	120
    1686	82	83
    1687	14	62
    1689	1	11
    1690	58	63
    1691	67	211
    1692	211	215
    1693	24	120
    1694	2	82
    1695	74	78
    1696	148	149
    1697	66	114
    1699	209	223
    1700	248	255
    1702	192	250
    1703	70	71
    1705	15	31
    1706	0	2
    1707	0	74
    1708	9	157
    1709	72	74
    1710	133	215
    1711	70	215
    1712	9	249
    1713	72	253
    1714	133	197
    1715	68	70
    1716	111	255
    1717	70	79
    1720	135	143
    1721	67	75
    1724	7	15
    1726	111	239
    1728	7	111
    1729	96	102
    1730	0	7
    1732	27	159
    1733	248	251
    1734	0	189
    1735	240	246
    1736	75	79
    1738	1	111
    1739	32	102
    1740	0	7
    1744	254	255
    1745	231	255
    1747	70	246
    1748	0	75
    1749	0	248
    1750	0	1
    1753	1	241
    1754	0	111
    1755	0	248
    1756	100	254
    1757	1	231
    1758	0	192
    1759	32	102
    1763	64	96
    1768	3	103
    1771	64	96
    1772	0	13
    1773	0	4
    1775	32	96
    1776	0	2
    1777	4	5
    1779	32	96
    1780	0	3
    1781	0	5
    1783	33	97
    1791	72	104
    1795	66	99
    1797	208	212
    1799	72	105
    1800	12	124
    1801	73	253
    1802	129	141
    1803	66	74
    1805	208	221
    1806	12	141
    1808	0	16
    1809	27	219
    1810	198	206
    1811	16	88
    1812	32	44
    1813	104	105
    1814	1	129
    1815	120	122
    1816	137	141
    1817	0	208
    1818	106	110
    1819	88	94
    1821	48	59
    1822	97	231
    1823	104	120
    1824	144	176
    1825	71	111
    1826	8	9
    1827	52	124
    1828	1	137
    1830	245	255
    1831	209	217
    1832	0	1
    1834	0	97
    1835	191	255
    1836	112	240
    1837	189	255
    1838	192	200
    1839	70	118
    1840	196	197
    1841	7	63
    1842	0	245
    1843	0	209
    1845	7	191
    1847	0	191
    1848	232	248
    1849	7	191
    1850	0	192
    1851	0	70
    1852	216	220
    1856	5	197
    1857	73	79
    1860	8	248
    1861	136	143
    1864	1	225
    1865	32	39
    1868	3	7
    1870	8	12
    1871	112	122
    1872	112	120
    1873	71	207
    1874	192	208
    1875	70	198
    1876	60	61
    1877	1	33
    1878	0	136
    1879	32	112
    1880	8	11
    1881	4	77
    1882	0	8
    1883	64	112
    1884	94	126
    1885	1	71
    1886	0	192
    1887	32	102
    1888	5	61
    1896	0	94
    1897	32	33
    1899	70	102
    1900	1	5
    1901	224	233
    1903	104	253
    1904	4	76
    1905	49	61
    1910	8	9
    1911	189	255
    1916	3	7
    1917	48	49
    1918	0	255
    1919	104	255
    1920	0	159
    1921	40	252
    1922	4	12
    1923	208	253
    1924	0	255
    1925	34	255
    1926	10	255
    1927	112	255
    1928	1	3
    1931	56	120
    1933	209	249
    1934	112	116
    1935	71	215
    1937	181	183
    1938	195	203
    1939	29	125
    1941	48	49
    1942	2	3
    1943	104	120
    1944	8	251
    1945	70	215
    1946	25	121
    1947	70	71
    1950	2	195
    1952	8	11
    1955	247	255
    1956	131	139
    1958	112	121
    1960	254	255
    1961	231	247
    1963	231	255
    1965	231	255
    1966	0	255
    1967	191	255
    1968	254	255
    1969	231	255
    1970	0	112
    1971	0	71
    1972	0	254
    1973	0	231
    1974	0	254
    1975	0	231
    1976	65	255
    1977	6	231
    1979	0	191
    1980	145	255
    1981	7	231
    1988	0	157
    1989	0	7
    1992	2	139
    1993	0	7
    2000	0	2
    2004	0	97
    2013	1	255
    2014	0	240
    	0
    1733	64	0
    1734	60	0
    1735	67	0
    1736	19	0
    1737	64	0
    1738	3	0
    1739	51	0
    1740	18	0
    1741	43	0
    1742	10	0
    1743	209	0
    1744	2	0
    1745	120	0
    1746	1	0
    1747	48	0
    1748	23	0
    1749	10	0
    1750	5	0
    1751	211	0
    1752	7	0
    1753	120	0
    1754	82	0
    1755	6	0
    1756	1	0
    1757	48	0
    1758	82	0
    1759	14	0
    1760	255	0
    1761	1	0
    1762	58	0
    1763	67	0
    1764	211	0
    1765	24	0
    1766	2	0
    1767	74	0
    1768	148	0
    1769	66	0
    1770	210	0
    1771	209	0
    1772	248	0
    1773	189	0
    1774	192	0
    1775	70	0
    1776	255	0
    1777	15	0
    1780	9	0
    1781	72	0
    1782	133	0
    1783	70	0
    1784	9	0
    1785	72	0
    1786	133	0
    1787	68	0
    1788	111	0
    1789	70	0
    1790	7	0
    1791	32	0
    1792	135	0
    1793	67	0
    1794	189	0
    1795	70	0
    1796	7	0
    1797	72	0
    1798	111	0
    1799	70	0
    1800	7	0
    1801	96	0
    1803	240	0
    1804	27	0
    1805	248	0
    1807	240	0
    1808	101	0
    1809	248	0
    1810	1	0
    1811	32	0
    1813	240	0
    1814	137	0
    1815	248	0
    1816	254	0
    1817	231	0
    1818	192	0
    1819	70	0
    1823	32	0
    1825	1	0
    1828	104	0
    1829	1	0
    1831	32	0
    1832	13	0
    1833	4	0
    1835	64	0
    1836	2	0
    1837	5	0
    1839	64	0
    1840	3	0
    1841	5	0
    1843	64	0
    1847	32	0
    1849	4	0
    1851	32	0
    1855	33	0
    1857	4	0
    1859	33	0
    1860	112	0
    1861	181	0
    1862	12	0
    1863	72	0
    1864	12	0
    1865	77	0
    1866	133	0
    1867	66	0
    1868	16	0
    1869	208	0
    1870	12	0
    1871	72	0
    1872	12	0
    1873	73	0
    1874	129	0
    1875	66	0
    1876	12	0
    1877	208	0
    1878	12	0
    1879	70	0
    1881	27	0
    1882	198	0
    1883	16	0
    1884	32	0
    1885	104	0
    1886	1	0
    1887	120	0
    1888	137	0
    1890	106	0
    1891	88	0
    1892	1	0
    1893	48	0
    1894	97	0
    1895	104	0
    1896	144	0
    1897	71	0
    1898	8	0
    1899	52	0
    1900	1	0
    1901	62	0
    1902	245	0
    1903	209	0
    1905	191	0
    1907	191	0
    1908	112	0
    1909	189	0
    1910	192	0
    1911	70	0
    1912	60	0
    1913	8	0
    1916	48	0
    1917	8	0
    1920	96	0
    1921	8	0
    1924	80	0
    1925	8	0
    1928	8	0
    1929	72	0
    1930	1	0
    1931	121	0
    1932	73	0
    1933	8	0
    1934	11	0
    1935	211	0
    1936	1	0
    1937	35	0
    1938	1	0
    1939	121	0
    1940	6	0
    1941	74	0
    1942	25	0
    1943	67	0
    1944	1	0
    1945	113	0
    1946	1	0
    1947	122	0
    1948	17	0
    1949	112	0
    1950	5	0
    1951	73	0
    1953	120	0
    1954	8	0
    1955	112	0
    1956	4	0
    1957	72	0
    1958	3	0
    1959	112	0
    1960	112	0
    1961	71	0
    1962	192	0
    1963	70	0
    1964	4	0
    1965	2	0
    1967	64	0
    1968	68	0
    1969	1	0
    1971	32	0
    1972	100	0
    1973	1	0
    1975	32	0
    1976	99	0
    1977	1	0
    1979	32	0
    1980	5	0
    1981	73	0
    1982	4	0
    1983	74	0
    1984	8	0
    1985	136	0
    1986	16	0
    1987	128	0
    1988	1	0
    1989	32	0
    1990	136	0
    1991	112	0
    1992	3	0
    1993	73	0
    1994	8	0
    1995	112	0
    1996	112	0
    1997	71	0
    1998	192	0
    1999	70	0
    2000	60	0
    2001	1	0
    2003	32	0
    2004	8	0
    2005	4	0
    2007	64	0
    2008	98	0
    2009	1	0
    2011	32	0
    2012	5	0
    2013	73	0
    2014	8	0
    2015	181	0
    2016	72	0
    2017	28	0
    2018	2	0
    2019	209	0
    2021	32	0
    2022	1	0
    2023	70	0
    2024	1	0
    2025	224	0
    2026	8	0
    2027	104	0
    2028	4	0
    2029	49	0
    2030	255	0
    2031	247	0
    2032	103	0
    2033	252	0
    2034	8	0
    2035	189	0
    2036	255	0
    2037	255	0
    2038	255	0
    2039	255	0
    2040	3	0
    2041	48	0
    2043	104	0
    2045	40	0
    2046	4	0
    2047	208	0
    2049	34	0
    2050	10	0
    2051	112	0
    2052	1	0
    2053	49	0
    2054	1	0
    2055	56	0
    2056	251	0
    2057	209	0
    2058	112	0
    2059	71	0
    2060	8	0
    2061	181	0
    2062	195	0
    2063	29	0
    2064	3	0
    2065	48	0
    2066	2	0
    2067	104	0
    2068	8	0
    2069	70	0
    2070	25	0
    2071	70	0
    2072	255	0
    2073	247	0
    2074	232	0
    2075	254	0
    2076	8	0
    2077	189	0
    2078	255	0
    2079	247	0
    2080	105	0
    2081	255	0
    2082	112	0
    2083	71	0
    2084	254	0
    2085	231	0
    2086	254	0
    2087	231	0
    2088	254	0
    2089	231	0
    2091	191	0
    2092	254	0
    2093	231	0
    2096	137	0
    2097	6	0
    2100	13	0
    2101	8	0
    2104	249	0
    2105	7	0
    2112	2	0
    2116	103	0
    2121	1	0
    2125	255	0
    2126	240	0
    2128	64	0
    2129	8	0
    2133	1	0
    2135	32	0
    2136	72	0
    2137	8	0
    2140	104	0
    2141	1	0
    2143	32	0
    

  • Hello,

    As I mentioned in the previous message, you do not need to program the DEVRAM if you are programming the OTP. To start with, I would try only programming the OTP with this procedure:

    • Close jumper 15.
    • Turn on external VCC. I have 24VDC
    • Open PGA900 utility.
    • Move to a Digital interface.
    • Send 0 to REMAP register
    • Load .hex to OTP memory
    • Verify OTP memory
    • Remove jumper 15
    • Move to a Microcontroller interface (the program should run)
    • Turn off external VCC
    • Turn on external VCC

    Another check you can perform is to see if your OTP is properly saved after resetting the device. Cycle the power, then go back to the memory page of the GUI and verify the OTP against your hex file. It should show a successful check.

    Regards,

  • Hi Scott.

    Thanks for your reply and your detailled information.
    I've been doing all your points but the problem was not solved.

    I've tried to remove the microcontroller and put other PGA900 and it runs ok!!!! So, the problem is solved. :)

    Thanks again Scott.