Dear TI support
I am using ARW1243 and TSW1400
I want to check that the Tx transmission signal (Frequency modulation:power, phase,chirp...) is exactly as in the design at sensorconfig by oscilloscope.The measurement block diagram is described in fig1.
fig1
but when performing steps 1-7 (fig2), I find that the current consumed on the AWR1243 board has not changed.
it is only 0.22A / 5V,
It does not change andtoo low compared to the source of contstream CW signal when streamenable :0.8A-1.1A / 5V.
I think my measurement has a problem.
I think my measurement has a problem.
Or it changes so fast and I can't see it.
fig2
And when I want to measure and store (data: ***. bin) a signal (not a CW signal) in about 5-10min, how should I do it?
Please show me how to do it right.
Thank you.
BUI GIAP