Other Parts Discussed in Thread: IWR1443
Hello,
currently I'm lloking for the protocol which is used for communication with the IWR1443 by the demo Applications (e.g. Visualizer).
What I'd like to do is, decoupling the XDS110 debug probe and directly interacting with the IWR1443.
The idea is to use a MCU's serial interface (UART) instead of the COM-Ports provided by the XDS110 via USB.
Could someone point me to where I could find a documentation about the protocol used by the IWR1443, maybe evan an API I might look at?
CCS: 9.0.1
SDK: 2.1 / 3.2
EVM: 3.0