This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1612EVM: I would like to express the operating principle of inductive sensor as a formula

Part Number: LDC1612EVM
Other Parts Discussed in Thread: LDC1612

We are studying inductive sensors using the LDC1612 EVM.
Could you explain the operation principle of inductive sensor with a formula?
(Quoting Maxwell's equation etc.)
Relationship between L and d (The conductivity, permeability, etc. of the target should be included in the parameters as well)
Please also use the capacitor used for the resonance circuit as a parameter