Other Parts Discussed in Thread: AWR1642,
Hello,
I have AWR1642 connected with DCA1000EVM and I am following the instructions present in the mmwave_studio_user_guide present in installation directory of mmwave_studio_02_00_00_02/docs/. By following the instructions I have issued reset to the board, connected the RS232 COM port and ran DataCaptureDemo_xWR.lua script. I am also observing output window. There is not even a single error from start of application in the output window. But in last i see a error when Packet_Recorder_Zerofill.exe is invoked by running script. The error is
The application was unable to start correctly (0xc000007b).
This is when i tried running application in admin user account.
When i tried running application in normal user mode then there is no error but the Packet_Recorder_Zerofill.exe open and just hangs there.
As per my knowledge the post processing step is having problem. MATLAB error is thrown because the adc_data.bin is not having any data. But adc_data_Raw_0.bin is a 4.03 MB file. Please kindly throw some light on this.
Thank you,