This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA460: Problems in ultrasonic robot application

Part Number: PGA460

HI team,

Please kindly help me check below three technical questions when using PGA460 in ultrasonic application.

1. How to adjust the analog front-end gain, is that using former sampling result as reference ?  If it was, how about the first sample gain?

2. How to suppress multiple channels ultrasonic interference? Is that right using different frequency in each channel or just encoding it before transmitting ? 

3. What should we consider when selecting transformer ? Does the ultrasonic frequency and transducer capacitor have effects on transformer selection?

Many thanks~

Stanley Dai.

  • Hi Stanley,

    Responding to your questions:

    1. The analog front end is time varying, hence time varying gain (TVG). The gain profile is predetermined by the user, and not based on preceding samples for reference (such as a log amp). A common time varying gain profile is to gradually increase the gain from an initial low gain level to a large gain level for long distance measurements. Take a look at the PGA460 ultrasonic sensing: EVM GUI device configuration video demo to see the TVG changes in action.

    2. The PGA460 does not include the DSP intelligence to suppress or differentiate various ultrasonic echos in the same frequency band of interest. Echo coding is not supported. For a system that is exposed to a noisy ultrasonic environment, I recommend that the time between each measurement iteration be randomized. This will allow for improved recognition of false positives caused by other ultrasonic sources.

    3. Transformer selection should be based on two parameters: transducer drive voltage rating and frequency.

    • If the transducer drive voltage rating is 50Vpp or greater, then a transformer driver is necessary to generate maximum sound pressure level for maximum ranging of the transducer. Typical ultrasonic transducer center-tap transformers will have a turns ratio of 1:1:10. The drive voltage can be fine-tuned and controlled by the center tap voltage supplied to the transformer and the PGA460 preset driver current limit value (50mA-500mA). 
    • If the frequency of the transducer is 30-80kHz, I recommend using a transformer with a 1~5mH secondary inductance rating. If the transducer frequency is 180-480kHz, I recommend using a transformer with a 100~500nH secondary inductance rating.
    • You can find a list of PGA460 compatible transducers and transformers at: http://www.ti.com/lit/zip/slac787
    • The matching values (tuning capacitor and/or damping resistor in parallel to transducer) will be impacted by the secondary inductance of the transformer, and the transducer's equivalent circuit. You will need to optimize these values based on your min/max range requirements.

  • Hi Akeem,

    Many thanks for your above reply. Here is a another question:

    Does the NO.14 pin (IOREG) can provide output current around 35mA as the voltage level of 5V?

    BR.

    Stanley Dai.

  • Stanley,

    Though IOREG is not intended to be used to drive external loads, it is possible to confiugre IOREG to 5V. Keep in mind that configuring IOREG to 5V will also configure TXD, RXD, and SCLK pins will also be referenced to 5V high logic.

    You need to connect an external 100kOhm pull up resistor from the TEST pin to 3.3V or 5V source to enable 5V at IOREG and the USART pins. See section 7.3.12 TEST Pin Functionality of the datasheet ( http://www.ti.com/lit/gpn/pga460-q1 ) for details.

  • Hi Akeem,

    Is that possible to measure ultrasonic wave whose frequency range is from 30 to 500 kHz using PGA460?

    If not, can you recommend one device for me? 

    Many thanks~

    BR.

    Stanley