Other Parts Discussed in Thread: IWR6843ISK, AWR1642, IWR6843
Tool/software: TI C/C++ Compiler
hi all
when i use IWR6843ISK_ODS , the CFG file of "mmw_pplcount_demo_overhead.cfg" just as below
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 0 1 1
profileCfg 0 60.6 100 7 40 0 0 82 1 128 5300 0 0 48
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 64 0 50 1 0
lowPower 0 0
cfarCfg -1 0 0 8 4 4 0 7000
cfarCfg -1 1 0 4 2 3 0 7000
SceneryParam -2.0 2 -0.1 3 -3 3
GatingParam 3 2 2 2 12
AllocationParam 100 80 0.2 15 2 12
StateParam 5 5 10 100 5
VariationParam 0.2887 0.2887 1 1
MaxAcceleration 0.1 0.1 0.1
AllocZone 0 1
CloudPersistence 0
trackingCfg 1 2 250 10 200 100 90
sensorStart
i find most of the parameters in the SDK file. but i can not find some of them in SDK file just as below
SceneryParam -2.0 2 -0.1 3 -3 3
GatingParam 3 2 2 2 12
AllocationParam 100 80 0.2 15 2 12
StateParam 5 5 10 100 5
VariationParam 0.2887 0.2887 1 1
MaxAcceleration 0.1 0.1 0.1
AllocZone 0 1
CloudPersistence 0
trackingCfg 1 2 250 10 200 100 90
So could you give me a paper to introduce this parameters .
Thanks