This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: OPT3101

Part Number: OPT3101

Hello,

I'd like to understand how does "tx_seq_reg" being set?

There is only an example found in datasheet, which is "register value: 2-1-0-2-1-0. The sequence will be 0-1-2-0-1-2"

But how is that being translated into 2Ah[14:3] ?

Hope i didn't ask a dumb question.

Best Regards,
Mike