This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Stuck on downloading MSS firmware

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: IWR1443, AWR1843

Hey Guys,

I am trying to take measurements using the AWR1843 and DCA1000. I was previously using IWR1443. With the AWR1843, I have downloaded mmWaveStudio 2.0.0.2. I can reset the board, connect for RS232, and download the BSS Firmware to the device. (I already flashed it). However, after trying to install the MSS firmware, the dialog box shows that 100% of the download is complete. But I cannot press the connect SPI and the the output is stuck on "Downloading MSS RPRC Binary. I don't know if this has to do with the firmware version. But I am using the same firmware located in the mmWaveStudio 2.0.0.2 folder.

The output is as shown below. I do not know what to do and am really stuck here.

GM: Constructor
GM: Mon Jun 17 16:40:23 2019
RSTD.Transmit("/Settings")
[16:40:23]
[16:40:23] ### Running Startup script: "C:\ti\mmwave_studio_02_00_00_02\mmWaveStudio\Scripts\Startup.lua" ###
[16:40:23] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[16:40:23] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[16:40:23] Scripter ignored: Attempt to UnBuild() again or before Build.
[16:40:23] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_00_00_02\\mmWaveStudio\\Clients\\\\LabClient.dll")
[16:40:23] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[16:40:23] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[16:40:23] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[16:40:23] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[16:40:23] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[16:40:23] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_00_00_02\\mmWaveStudio\\RunTime\\SAL.dll")
[16:40:23] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[16:40:23] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[16:40:23] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[16:40:23] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[16:40:23] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[16:40:23] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[16:40:23] RSTD.Transmit("/")
[16:40:23] RSTD.SaveSettings(): Settings saved to "C:\Users\bru170000\AppData\Roaming\RSTD\config.xml"
[16:40:23] RSTD.Build()
[16:40:23] RSTD.SaveSettings(): Settings saved to "C:\Users\bru170000\AppData\Roaming\RSTD\config.xml"
[16:40:23] RSTD.Transmit("/")
[16:40:23] RSTD.AL_Build()
[16:40:23] RSTD.AL_LoadXml()
[16:40:23] RSTD.Transmit("/")
[16:40:23] RSTD.AL_Init()
[16:40:23] RSTD.Clients_Build()
[16:40:23] GM: Init
[16:40:23] GM: Loaded 'C:\ti\mmwave_studio_02_00_00_02\mmWaveStudio\Clients\\LabClient.dll'
[16:40:23] GM: 1 Guest (s) init
[16:40:23] GM: 1 Module(s) init
[16:40:23] GM: 2 Tab (s) init
[16:40:23] RSTD.Client_LoadXml()
[16:40:23] [RadarAPI]: Starting Matlab Engine..
[16:40:27] [RadarAPI]: Matlab Engine Started!
[16:40:29] [RadarAPI]: ar1.LoadSettings('C:\Users\bru170000\AppData\Roaming\RSTD\ar1gui.ini')
[16:40:30] TESTING = false
[16:40:30]
[16:40:30] ***Script completed successfully.***
[16:40:39] [RadarAPI]: Opening Gpio Control Port()
[16:40:39] [RadarAPI]: Status: Passed
[16:40:40] [RadarAPI]: Opening Board Control Port()
[16:40:40] [RadarAPI]: Status: Passed
[16:40:41] [RadarAPI]: ar1.FullReset()
[16:40:41] [RadarAPI]: Status: Passed
[16:40:41] [RadarAPI]: Closing Board Control Port()
[16:40:41] [RadarAPI]: Status: Passed
[16:40:41] [RadarAPI]: Closing Gpio Control Port()
[16:40:41] [RadarAPI]: Status: Passed
[16:40:41] [RadarAPI]: ar1.SOPControl(2)
[16:40:41] [RadarAPI]: Status: Passed
[16:40:48] [RadarAPI]: ar1.Connect(15,115200,1000)
[16:40:49] [RadarAPI]: ar1.Calling_IsConnected()
[16:40:50] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[16:40:50] [RadarAPI]: Status: Passed
[16:40:50] [RadarAPI]: RS232 is not connected ..!!!!
[16:40:50] [RadarAPI]: ar1.frequencyBandSelection("77G")
[16:40:50] [RadarAPI]: ar1.SelectChipVersion("XWR1843")
[16:40:50] [RadarAPI]: Status: Passed
[16:40:50] Device Status : XWR1843/ASIL-B/SOP:2/ES:2
[16:40:51] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[16:40:51] [RadarAPI]: Status: Passed
[16:40:51] [RadarAPI]: ar1.SelectChipVersion("XWR1843")
[16:40:51] [RadarAPI]: Status: Passed
[16:40:51] Device Status : XWR1843/ASIL-B/SOP:2/ES:2
[16:40:51] [RadarAPI]: ar1.SaveSettings('C:\Users\bru170000\AppData\Roaming\RSTD\ar1gui.ini')
[16:41:31] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_dfp_01_02_00_01\\rf_eval\\rf_eval_firmware\\radarss\\xwr18xx_radarss_rprc.bin")
[16:41:31] [RadarAPI]: Downloading BSS Patch RPRC Binary..
[16:41:38] [RadarAPI]: ar1.GetBSSFwVersion()
[16:41:38] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[16:41:39] [RadarAPI]: ar1.GetBSSPatchFwVersion()
[16:41:39] [RadarAPI]: BSSPatchFwVersion:(01.02.00.03 (24/10/18))
[16:41:55] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_dfp_01_02_00_01\\rf_eval\\rf_eval_firmware\\masterss\\xwr18xx_masterss_rprc.bin")
[16:41:55] [RadarAPI]: Downloading MSS RPRC Binary..

After this, nothing happens at all. I would be grateful if somebody could help me out. 

Best regards,

Bhaskar Raj Upadhyay