This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: Where to download the AWR1243BOOST SDK?

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: AWR1243, AWR1642

Hi Team,

The 2.0 version of the SDK downloaded by the customer has only 14 and 16 without 12. The customer wants to read the data measured in AWR1243BOOST, how to achieve it? Does he need to write a C++ program to call the program inside the SDK, how to call it?

Thanks.

  • Hi Annie,

    The AWR1243 is only a front-end with no processing capability. So there is no SDK for this device.

    There is example code for the AWR1243 provided as part of the Device Firmware Package (DFP) which is available here:

    Please also refer to our training videos available here which cover the different parts and software components in Section 2:

    Best Regards,

    Anand

  • Hi Anand,

    Thanks for your support. 

    If the customer wants to use ARW1642BOOT, how to write a c++ program to call the front-end program inside 1642, and read the result?Is there a case or video?

    Appreciate for your help in advance. 

  • Hi Annie,

    For the AWR1642, please refer to our mmWave SDK, available from here:

    Please go through the training videos as they cover all of these questions.

    Best Regards,

    Anand