This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA305: Question for PGA305

Part Number: PGA305

Hi Team,

Customer wants to know how to set the internal ADC sampling period of the PGA305? There is no description in the datasheet. Only the ADC clock frequency is 1MHz. Is there any way to confirm the sampling frequency?

PARAMETER MIN TYP MAX UNIT
Sigma-delta modulator frequency 1 MHz
ADC voltage input range –2.5 2.5 V
Number of bits 24 bits

Thanks.