This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR1642BOOST-ODS: SRR demo velocity estimation issue

Part Number: AWR1642BOOST-ODS
Other Parts Discussed in Thread: AWR1642BOOST

Tool/software: Code Composer Studio

Hi

I’m trying to work with SRR demo using awr1642boost-ods. The board is in a room which all of the objects are static, but as u can see in Doppler-Range plot it shows that there are obstacles with approximately -11m/s velocity. The configuration is set for USRR (one subframe) which has the maximum range of 20 meters and maximum velocity of 5m/s (18km/h) so it shouldn’t show -11m/s in any scenario. Can anybody please help me with this?

Thanks