This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000: No signal at RX side

Part Number: TDC1000

Hello guys,

I'm using TDC1000 with 300 KHZ multifeed sensors.
I'm able to TX 5 pulses of 300khz with 10v amplitude .

but at receiving end i'm not able to receive signal.

but when i attach that sensor individually directly with DSO probe then i'm able to receive signal of 10 to 20mV at 5 to 20cm distance.

but when i attached that sensor with circuit i'm not able to receive any signal even at same distance.

is it ground problem?or other

please help

Thanks