This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1642BOOST: Which file allows access to the Allocation Parameters for the Point Threshold, SNR Threshold and Det2Active Threshold

Part Number: IWR1642BOOST


Tool/software: Code Composer Studio

Hi All,

I'm a bit new with the IWR1642BOOST and CCS, so please bear with me. I am trying to manipulate the Person Counter Lab to eliminate Ghost Detection. However, I don't know where I can access the parameters referenced by the People-Counting Tuning Guide:

1) Allocation Parameters – SNR Threshold
2) Allocation Parameters – Points Threshold
3) State Transition Parameters – Det2Active Threshold
4) State Transition Parameters – Det2Free, Static2Free, Active2Free, exit2Free

I have CCS downloaded with the DSS and MSS opened, anything is appreciated. Thanks!