Hi:
I want to use PGA900 for load cell.
Can I use DAC loop back to calibrate output of PGA900 ?
Is it possible? Could it be very accurate ?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
I want to use PGA900 for load cell.
Can I use DAC loop back to calibrate output of PGA900 ?
Is it possible? Could it be very accurate ?
thanks
Hello,
Yes, you can use the loopback feature to calibrate the DAC output of the PGA900 if you wish. The details of the loopback operation are found in the DAC Diagnostics section of the PGA900 datasheet.The accuracy of the measurement is just limited by the 24 bit resolution of the ADC.
Regards,