I've managed to write a script that can send configuration commands to the DCA1000EVM. However, it still requires the Trigger Frame button to be pushed manually in mmWave Studio. I saw that it is possible to connect a hardware trigger for this function, but is there any way to send a command to begin this process through software, such as from my python script.
Furthermore, my implementation also requires all 6 buttons on the Connection tab within mmWave Studio to be pressed; is there a way to do this with commands as well?
Thanks,
Pawel