This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: Powering up the AWR1443 board

Part Number: AWR1443BOOST
Other Parts Discussed in Thread: AWR1443

Hello All

I am using a 5V-2.5A adapter to power the AWR1443 board but now I want to switch to power bank to power it up which can give up to 2A. Is there any problem I might face or is there any chance that under powering the board might damage it??

Hoping for Quick Response

Thanks and Regards

Yashutosh

  • Hello,

    5V - 2A should be OK. It will not damage the board. But do use a good quality power bank. Some power banks mention 2A load capacity but are not able to actually provide that current. In which case you might see poor performance from the radar.

    Regards,

    Vivek