This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: Using mmWave SDK 3.02.00.04 with IWR6843ISK-ODS

Part Number: IWR6843ISK-ODS

Hi,

I have a setup with the IWR6843ISK-ODS board and I am interested in the raw data output of the sensor. I already followed the instructions of the “ODS Point Cloud User Guide” and it seems to work fine for me. I use an own application to read out the raw data from the sensor. The x,y,z-coordinates of the detected objects makes sense for me.

Now, I want to try out the mmWave SDK. I use the version 3.02.00.04. The setup is the same as before. However, the resulting x,y,z-coordinates of the detected objects makes no sense to me.

I know that the output format of SDK and ODS application is different what I respect in my application. There is also the recommendation to use the “ODS Point Cloud User Guide” in the thread http://e2e.ti.com/support/sensors/f/1023/t/794127?IWR6843ISK-ODS-Which-verison-of-MMWAVE-SDK-can-support-IWR6843ISK-ODS- because the visualization is different.

Is the visualization different due to incorrect raw data (x,y,z coordinates) from the SDK, which means that the SDK cannot be used with the IWR6843ISK-ODS?

Cheers,

Tony