Other Parts Discussed in Thread: IWR1642
Tool/software: Code Composer Studio
Hi,
Is there any way to Increasing people detection range in lab0011-pplcount over 14m, I tried to change the cfg file but nothing gave good results.
Attached my cfg thats works for 14m:
'dfeDataOutputMode 1',
'channelCfg 15 3 0',
'adcCfg 2 1',
'adcbufCfg 0 1 1 1 ',
'profileCfg 0 77 30 7 62 0 0 24 1 128 2500 0 0 30',
'chirpCfg 0 0 0 0 0 0 0 1',
'chirpCfg 1 1 0 0 0 0 0 2',
'frameCfg 0 1 128 0 50 1 0',
'lowPower 0 1',
'guiMonitor 1 1 0 0',
'cfarCfg 6 4 4 0 0 16 16 4 4 50 62 0',
'doaCfg 600 1875 30 1',
'SceneryParam -12 12 0.05 16',
'GatingParam 4 3 2 0',
'StateParam 5 5 10 100 5',
'AllocationParam 100 0.01 8 1 2',
'VariationParam 0.289 0.289 1.0',
'trackingCfg 1 2 250 20 200 50 90',
'sensorStart'.
What should I change in order for it to detect up to 40m?