This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS / IWR1443BOOST:IWR1443BOOST

Part Number: IWR1443BOOST

Tool/software: Code Composer Studio

Hi,

When I did an area occupancy test with the IWR1443BOOST, I noticed that there were a lot of interfering objects when I tested the electrical objects. What happened?Is it electromagnetic interference?If so, how do you eliminate this interference?

Greetings,

Li

  • Former Member
    0 Former Member

    Hello,

    Can you provide more details about what you mean when you refer to testing electrical objects and the problems you see.

    If you are concerned about interference you could replicate the testing with the items unpowered and powered to see if you observe the the same results.

    Please note that metallic items are highly reflective for mmWave sensors and this could be instead be what you are observing if your electronics are mainly comprised of metal. If you want to ignore these objects then you can enable the static clutter removal - this would only allow you to detect moving objects then.

    Amanda