Other Parts Discussed in Thread: AWR1843BOOST, AWR1642
Hello everyone,
As you know, TI DemoVisualizer provides two operating frequency bands: 1) 76-77GHz and 2) 77-81GHz.
For our case, We would like to use AWR1642BOOT and AWR1843BOOST in different operating frequency bands. In that respect, we have created a new configuration, which sets start frequency to 77GHz with 1GHz bandwidth. We were able to start the sensor with our new configuration; however we have noticed that start frequency of AWR1642 has not changed it to 77GHz after we run chirp analysis in our spectrum analyzer.
So our question is:
- Can those boards only support operating frequency bands: 1) 76-77GHz and 2) 77-81GHz or select one of them as default?
- Is there any way to modify operating frequency bands, e.g. modifying firware etc.?
Thank you for your support.