Part Number: IWR6843
Other Parts Discussed in Thread: DCA1000EVM
Hello,
I have referred the "Antenna Database" section from the following TI website link: http://www.ti.com/sensors/mmwave/iwr/applications/applications.html
For the 60GHz standard antenna on IWR6843ISK, maximum detectable range for a car is mentioned as 175m and for a person, it is 98m.
To achieve this results, which is the firmware and configuration required and is it tested with the person or corner reflector of the same RCS?
Also, Is there any trade off between range and performance(detection time) to achieve this?