This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: Using RED Laser diode instead of LED

Part Number: OPT3101


Hi,

Could you please tell me whether the following RED Laser diode can be used instead of LED which is used on OPT3101EVM ?

How can I control the illumination currrent to 25mA ~ 30mA?

Best regards,