This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pins and terminations required to run the LRPC demo

Part Number: IWR6843ISK


What is the minimum ISK I/O connections/terminations required to enable reliable operation of the ISK?  Are they?:

Supply 3.3V power rail.
Terminate SOP0 with PU to 3.3V
Terminate SOP1 with PD to GND
Terminate SOP2 with PU to 3.3V. GND to program
Terminate NRST with PU to 3.3V. GND to reset and begin execution of LRPC demo if programmed.
Terminate WARMRST with PU to 3.3V
Bring out RS232TX/RX as the "UART" channel as the setup for the LRPC demo.
Bring out MSS_Logger TX as the "Data Port" output to the LRPC demo.

Specifically are there ANY other pins that require attention while attempting to run the LRPC Demo?