This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Add the CAN-FD interface in AWR1843boot

Part Number: AWR1843BOOST


Hi TI team

I want to add the CAN-FD interface into AWR1843boot.

The origin schematic TI provided seems to only use CAN interface by TCAN1042HGVDQ1 and TS3A5018RSVR.

If I want to add CAN-FD, what do I need to add into the schematic of AWR1843boost?

Do you have recommended schematic of CAN-FD which can be combined with AWR1843boost?