This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Phase shift in TX path

Part Number: IWR6843

How can I get information about the possible timing of the phase shift  in the TX path (e.g. in case of a BPSK)

What is the minimum and maximum frequency and how can I control this frequency.

Best reagards Michael

  • Hello,

    the given link explains only that the chipset supports phase modulation (e.b. BPSK) "Transmitter Phase control: The transmit chains support Binary Phase Modulation (0 or 180 degree) which again is controlled using an API provided in the mmWave SDK. (There are actually 3 independent transmit chains on the IWR6843 so the TRM needs a minor correction.)"

    This Information was well known before, but my question is about the timing limitations. What is the minimum and what is the maximum modulation frequency? The link to the software SDKs is not helpfull, because I'll need this information before I will start ordering the chip and the sdk tools.

    I hope you can sent me the requested min and max modulation frequencies of the Phase control.

    Best regards

    Michael Thiel

  • Hello,

         For every chip you could have BPM (Binary phase shift modulation) bit is allocated per transmitter.

    Chirp could have FMCW modulation frequency from 60GHz to 64GHz . BPM bit could take only two values 0 deg or 180 Deg only within the chirp. 

    Thanks and regards,

    CHETHAN KUMAR Y.B.

  • Sorry for my next try.

    My questing was not about the frequency band. This was very clear from the beginning and is wirttenin the data sheet. My Question is about modulation (BPM) frequency.  Does it mean that the BPM frequency is for FMCW similar to the to the chirp frequency and what is the limitation in the  special case, if   the chip is working in CW mode and operate only with a BPM (e.g. measurement of velocity). In case of very slow speeds, I will have very low Doppler frequencies and therefore I can use a BPM modulation to build a heterodyne system (receiver support I/Q). in this case it is import to know the frequency range of the BPM modulation.

    best regards

    Michael

  • Michael, 

          BPM is not supported in the CW mode. BPM is supported only in the chirping mode.

    Could you please elaborate your application? 

    Thanks and regards,

    CHETHAN KUMAR Y.B.