Hi,
I am using the FDC2214 for liquid level sensing and the input range is about 10nF to 200nF(the sensor contacts the water directly and the capacitor is large).
TI suggests the typical choice is 18uH + 33pF. I think this choice is for input range at several pF.
1. How to ensure the Vsensor is at 1.2V~1.8V?
2. For capacitor about several hundred nF. I want to select the origin LC tank as 47nH + 10nF. Is that more suitable for my application?
Looking forward for your reply.
Best regards,
Di