This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: Phase drift of TxRx channels in MIMO mode

Part Number: AWR1243


Hi,

With all internal calibration of the awr1243 enabled what would be a reasonable expectation of the RMS phase drift over time of TX-Rx pair signals path within+-10 C of ambient (e.g. 20C ) temperature.

Thank you,

Vladimir Kolinko.

  • Hello Vladimir,

    Within a +-10deg temperature range the phase drift of Tx-Rx pair would be very small . But if you have the run time calibrations enabled and if the temperature crosses a boundary where the gains a changed internally then there could be large phase jump (in absolute terms) at that point. This jump would be seen across all the Tx- Rx pairs of the device , so typically its not an issue. But incase its an issue for your application you can disable the run time calibrations to avoid any phase jump.

    regards,

    vivek