Hello,
I am thinking of using IWR1443BOOST EVM or IWR6843ODS EVM for gesture detection purpose.
My requirement is for left,right,up and down swipe. In IWR1443BOOST EVM, it has only one gesture left-right-left sensing.
Or should I use IWR6843ODS EVNM which has source code for detecting two gesture i.e. left swipe and down swipe. But this EVM has additional feature of movement detection.
Is it possible to make changes in the source code available on the site of Ti and make it usable for the mentioned four gestures.
If yes can you provide the source code for additional gestures ?
Which EVM should i go with for easy understanding as I am doing this project for gesture detection for the first time.
Thank & Regards,
Yash