This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Medium Range Radar

Part Number: AWR1843BOOST

What is the maximum number of objects that the MRR project can detect?

http://dev.ti.com/tirex/explore/node?node=AObIl5yAPR-DjIwxgdgyuA__AocYeEd__LATEST

  • Hi,

    Could you provide the backgrounf for this question?

    In this type of processing chain the number of objects that can be detected is only related to the memory size used to store the array of detected objects (x,y,z, velocity)

    So, this is usually not a limitation.

    The limitation in the detected points comes from other system factors such as SNR, peak detection ...

    Thank you

    Cesar