Other Parts Discussed in Thread: TDA2, AWR1243, AWR1642, AWR1843
I want to use at-least 4 AWR1243BOOST EVMs simultaneously (1 for Long range(upto 300 m), 1 for Mid Range(80-150 m ), 1 for short range(10-80 m) and 1 for ultra short range(<10 m).
As the AWR1243BOOST doesn't have an on-board DSP as well as Microcontroller, which will the best suited processor for it?
Can i use TDA2x or TDA3x to interface all the four AR1243BOOST devices simultaneously?
If there a reference design or implementation of using multiple radar please share.
Is there any approach for using multiple radars EVMs simultaneously?
Regards,
Rahul Kumar