This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Configure the IP address of virtual machine with DCA1000EVM

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843, DCA1000EVM,

Hi,

I am trying to run the DCA1000 and AWR1843 EVM under a windows10 virtual machine system (VMware workstation). I set the IP address to 192.168.33.30 in virtual machine according to the DCA1000 Quick Guide. However, it doesn't work when I try to connect the ethernet. The mmwave studio shows error 'Ethernet cable is disconnected, please check'. That is pretty weird, because I can succeed connecting ethernet and capturing data with the same board but in the host system.

Do you have any idea of configuring DCA1000 and IP address in virtual machine system?

Thanks,

William