This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: What is the maximum sampling rate configuration (hence range from beat signal) possible with the demo visualizer app

Part Number: AWR1642

The maximum range (best range measurement ) possible using the demo visualizer is limited to 50 m. Can this be extended further. The AWR 1642 datasheet says that the device can be used for LRR mode also by programming the chirp parameters. Is it possible in the demo visualizer app?